Do not connect OPC shutdown interface
Determines the behaviour of the variable server when the OPC server application is shut down. If the OPC server is shut down while the variable server connected as a client is running, this can be reported to the variable server via the shutdown interface.
|
Setting |
Description of the |
|---|---|
|
|
The message via the shutdown interface of the OPC server is ignored. An error is generated. |
|
|
The message about the shutdown interface of the OPC server is recorded. The variable server then attempts to re-establish the connection. |
Parameters for module: