Protectrecipe from manipulation

If this parameter is activated, a checksum of the content and the name of the file is created using a complex formula when the recipe file is saved and saved in the header of the file. When the recipe file is loaded, the system checks whether the checksum is correct. If not, FileCorrupted is returned and the file cannot be loaded. The checksum enables modifications to the content and name of the recipe file to be recognised.
Figure 1 : If an XML recipe file has been manipulated externally, an error message is displayed at the top of the alarm line and in the RecipeView under "Status:" when an attempt is made to load the file.

Parameters for

Recipes module:
Recipe class (only standard serverfrom version 7.3 SP1)