Recipe name variable SPS
During the datatransfer actionsSend and Write, recipe data is written to the variable server and therefore usually to the PLC.
- Send
- The content of a recipe file is transferred directly to the variable server by specifying the recipe name.
- Writing
- The content of the recipe buffer is transferred to the variable server. In this case, the recipe name is normally available in the recipe buffer management, as a recipe file was previously loaded. If the recipe buffer is reinitialised, an empty text is used as the recipe name.
The recipe name is written to the variable specified in this parameter. The name is also available in the information block for the process.
Parameters for
- Recipes module:
- Recipe class