Variable for write trigger
Defines a variable whose value change to 1 triggers the writing of values from the recipe server to the variable server. After writing, the value of the variable is automatically reset to 0. The variable can have either a Boolean or an integer data type. The bit serving as the trigger is then selected by specifying the bit number in the variable selection dialogue.
Parameters for
- Recipes module:
- Recipe class