Information block (recipe data)
Contains metadata about the processing of a recipe.
Various information is recorded when a recipe is processed, e.g. who loaded which recipe and when. The recipe class manages three different information blocks in the recipe class object at runtime. The name of the associated property in the recipe class object is given in brackets.
- Process (LastRecipeSentToProcess)
- When and by whom was the content of the recipe buffer (only the variable values) last transferred to the variable server?
- Buffer (LastRecipeLoadedToBuffer)
- Which recipe file was last loaded into the recipe buffer?
- File (LastRecipeSavedToFile)
- In which recipe file was the recipe buffer last saved?
The following data is saved in the information block:
- Recipe name
- The name of the recipe that was specified when loading or saving.
- Description of the
- A freely usable description of the recipe content. This can be entered in addition to the recipe name when saving and is also reloaded from a recipe file back into the recipe buffer.
- User name
- The login name or full name of the operator from the user administration who triggered the action (save, load, write) for the recipe.
- Timestamp
- Date and time when the operator triggered the action for the recipe.
- Directory
- Directory in which the recipe was saved.
- Computer name
- Computer name on which the action for the recipe was triggered.