Recipe class object
The recipe class object in the VisiWin API provides programmatic access to a recipe class.
A recipe class object is linked to a recipe class in the server. The various data can then be accessed via its interfaces or information about the current status of a recipe can be retrieved.
Note: Depending on the UI technology, the names of the objects, properties and methods differ in the VisiWin API:
Classic UI
| Recipe class object | RecipeClass |
| Retrieval and initialisation | RecipeClass recipeClass = RecipeManager.Classes[recipeClassName];
|
- See also
- RecipeClassHandler (component)
Modern UI
| Recipe class object | IRecipeClass, RecipeClass |
| Retrieval and initialisation | IRecipeService recipeService = ApplicationService.GetService<IRecipeService>(); IRecipeClass recipeClass = await recipeService.GetRecipeClassAsync(recipeClassName); |
- See also
Web UI
| Recipe class object | IRecipeClass, RecipeClass |
| Retrieval and initialisation | const recipeService = VisiWin.System.Recipe.RecipeService.getService();const recipeClass = await recipeService.GetRecipeClassAsync(recipeClassName); |
- See also
- IRecipeClass (interface)