Add images to the project

A new Web UI client project already contains a number of images in the images folder within the project directory. This guide shows you how to add images to the project.

  • To add an image to the project:

  1. In the Project Explorer, expand the folders [ProjectName]_Client > Design > images.

  2. Right-click on the bitmaps, svgicons or svgs folder, depending on the type of the image you want to add, and select Add New Image... from the context menu.

    The Choose Image dialog appears.

  3. Navigate to the location of the image you want to add.

  4. Select the image and click on Open.

A copy of the image is now located in the folder you selected in step 2 and the image file name appears in the Project Explorer in the IDE. To show the image in a control, select the control in the Designer or in the Document Outline and select the image in an image property (Image, Symbol, etc.) of the control.

Related topics: