Images

Display of one or more graphics in a control element.

A graphic can be displayed in a control element in addition to the text or labelling.

Some controls can display one or more graphics.

The following types of graphics are possible:

Checkmark symbol

Graphic that is displayed in the checkbox of the Checkbox control element. The properties for configuring the graphic can be found in the "Checkmark" category.

Concerns control element: Checkbox

DefaultSymbol

Graphic that is displayed in the control if no graphics have been defined in the AlarmIndicatorItems or if all alarms of the classes to be displayed are in the inactive state (cleared).

Concerns control element: AlarmIndicator

ErrorSymbol

Graphic that is displayed behind the input field of the control in the event of an error, e.g. if the input is outside the specified limits. The properties for configuring the graphic can be found in the "ErrorSymbol" category.

Affects controls: DateTimeVarIn, NumericVarIn, TextVarIn

ExpandingSymbol

Graphic that is displayed when the selection list is collapsed ("CollapsedSymbol") or opened (ExpandingSymbol). The properties for configuring these graphics can be found in the "ExpandingSymbol" category.

Concerns control element: TabMenuButton

LabelSymbol

Graphic that can be displayed in addition to the label ofthe SelectBox. The properties for configuring the graphic can be found in the "LabelSymbol" category.

Subject control: SelectBox

LeadingSymbol

Graphic that is displayed in front of the output/input field of the control element. The properties for configuring the graphic can be found in the "LeadingSymbol" category.

Affects controls: DateTimeVarIn, DateTimeVarOut, DropDownBox, NumericVarIn, TextVarIn

Symbol

Graphic that can be displayed in addition to the labellingor text of the control element. The properties for configuring the graphic can be found in the "Symbol" category.

In the SelectBox, this is the graphic that is displayed in front of the text field containing the main and secondary text. At runtime, the graphic that has been configured for the active SelectBox item is displayed.

Concerns controls: Button, DateTimeVarIn, DropDownBox, DropDownBoxItem, Key, Label, ListItem, NumericVarIn, NumericVarOut, SelectBox, SelectBoxItem, StateIndicator, StateIndicatorItem, TabButton, TabMenuButton, TextVarIn, TextVarOut, ToggleButton

SymbolActive, SymbolInactive

Graphic that is displayed when an alarm of the alarm class specified in the "AlarmClassName" property has changed to the "Incoming" ("SymbolActive") or "Outgoing" (SymbolInactive) state. The properties can be found in the "Symbol" category.

Concerns control element: AlarmIndicatorItem

StateSymbol

Graphic that is displayed when the selection list is collapsed ("ClosedStateSymbol") or open (OpenedStateSymbol). The properties for configuring these graphics can be found in the "StateSymbol" category.

Subject control: SelectBox

Trailing symbol

Graphic that is displayed behind the input field of the control element. The properties for configuring the graphic can be found in the "Trailing symbol" category.

Subject: "DropDownBox, NumericVarIn, TextVarIn

Properties for configuring the graphic

For a control element that supports the display of a graphic (a symbol), the graphic can be configured using the following properties.

Example: The "ShowSymbol" property specifies whether the graphic of type Symbol should be displayed in the control, just as the "ShowErrorSymbol" property specifies whether the graphic of type ErrorSymbol should be displayed.

SymbolType

Defines the graphic type and the source of the graphic.

IconFont

Defines the graphic collection for the "Icon" graphic type.

ShowSymbol

Determines whether the graphic is to be displayed. The graphic to be displayed is defined in the "Symbol" property.

Symbol (SymbolOff/SymbolOn)

Defines the graphic to be displayed. The button opens a dialogue in which you can select one of the available graphics.

SymbolMargin

Defines the outer spacing of the graphic, i.e. between the edge of the graphic and its parent or neighbouring element.

SymbolPosition

Defines the position of the graphic in the containing (internal) container within the control element.

SymbolPressed

Defines the graphic that is displayed in the control element as long as it is held down ("Pressed"status ).

SymbolSize

Determines the display size of the graphic. The graphic is always displayed in a square (SymbolSize = width = height) and scaled to the set display size. As the CSS properties "width" and "height" are used internally for the graphic, all specifications that are permitted for these CSS properties are permitted in "SymbolSize", e.g. px, cm, % etc. If a number without a unit is entered as a value, this is interpreted as a specification in pixels.