Button

Button for calling up a function.

Symbol

Menu ribbon

Start > Controls > Buttons > General > Button (Default/Icon/Flat)

The "Button" control element is used to trigger an event by pressing it with the mouse, keyboard or finger, in which any function can be called up. The operation (press/release) is graphically animated, e.g. with shadow effects and colour changes.

The button when not pressed and when pressed

Functionalities

The control element supports the following functionality:

You can configure these functionalities via the properties in the Properties window when you select the control in the Designer or in the document outline. Whether a property is visible in the properties window depends on the style of the control.

Style

For demonstration purposes, the control element in the ribbon is available in three styles: "Button (Plain.Default)", "Button (Plain.Icon)" and "Button (Plain.Flat)". Further system styles are available for the control element in the "Style" property from the "General properties" category.

Certain properties may be missing in the Properties window for styled controls. For example, the "Colours" category is not available for controls in the system styles. These properties cannot be edited in the system styles.

You can also create your own styles for the control element. These styles are available for selection in the "Style" property after creation.

Structure

The control element consists of a number of other elements. Both the control itself and its elements can be configured via the properties of the control. Properties for a sub-element of the control can usually be found in the category that bears the name of this element.

Example: The properties for configuring the "Text" element can be found in the Properties window in the "Text" category when you select the control element in the Designer or in the document outline.

The button and its elements

Related topics: