TextVarIn

Input/output field for an alphanumeric process variable value.

Symbol

Menu ribbon

Start > Controls > Input/output > Variable input > TextVarIn

The "TextVarIn" control element is used to transfer an alphanumeric process variable value between the application interface and the variable server.

Example: The TextVarIn can be used to enter text or passwords. In the latter case, the characters entered are masked by dots.

TextVarIn with text input and TextVarIn with password input

Functionalities

The control element supports the following functionality:

You can configure these functionalities via the properties in the Properties window when you select the control in the Designer or in the document outline. Whether a property is visible in the properties window depends on the style of the control.

Style

By default, the control uses the "Plain.Default" style. Other system styles are available for the control in the "Style" property from the "General properties" category.

Certain properties may be missing in the Properties window for styled controls. For example, the "Colors" category is not available for controls in the system styles. These properties cannot be edited in the system styles.

You can also create your own styles for the control element. These styles are available for selection in the "Style" property after creation.

Structure

The control element consists of a number of other elements. Both the control itself and its elements can be configured via the properties of the control. Properties for a sub-element of the control can usually be found in the category that bears the name of this element.

Example: The properties for configuring the "Label" element can be found in the "Properties" window in the "Label" category if you select the control element in the Designer or in the document outline.

The TextVarIn and its elements

Input field (Input, InputContainer, ...)

The TextVarIn contains an input field into which a text can be entered at runtime.

If the style of the TextVarIn is reset, the following can be configured via the properties of the "Input" category:

The following illustration shows how the elements are structurally connected and which properties affect which element:

InputContainer and its elements

Related topics: