Reference value
Start value for the ring or bar in the output control element.
The reference value is the value within the valid value range from which the ring or bar is drawn.
A bar is drawn in the Bar control (LinearRange) and a ring is drawn in the RadialInstrument (RadialRange).
Reference value for the radial instrument and the bar
The reference value is defined via the "RawReferenceValue" property in the "ReferenceValue" category. By default, this property contains the value 0.
Affects these controls: