Region
Container for dynamic loading of views.
| Symbol |
|
| Menu ribbon |
- must have a name so that views can be dynamically loaded into the region via navigation buttons
- When assigning a name, the field sometimes does not accept the input, then assign a different name
- ViewName specifies the view that is displayed if no view is dynamically loaded into the region via navigation buttons. If a view is specified in StartView in a tab bar that is linked to this region, the view specified in the region via ViewName is ignored.
- no styles