User interface language

Definition of the user interface language.

If the translation manager is copied to a computer on which VisiWin is not installed, this setting can be used to set the language of the user interface. This requires a restart of the programme. The languages "German" and "English" are supported.

This setting is not available on computers with VisiWin installed. The translation manager then uses the same language that is set in VisiWin. The setting can be found there under the menuExtrasOptionsDevelopmentenvironmentGeneralLanguage.