This FB serves to read the current position of the axes group in the selected coordinate system.
- This is an administrative FB as no motion command is generated.
|
|
|
|
MC_GroupReadActualPosition |
|
|
|
|
|---|---|---|---|---|---|---|---|
|
AXES_GROUP_REF |
- |
|
AxesGroup |
Valid |
|
- |
BOOL |
|
BOOL |
- |
|
ENABLE |
Busy |
|
- |
BOOL |
|
L_MC4P_CoordSystem |
- |
|
CoordSystem |
Error |
|
- |
BOOL |
|
|
|
|
|
ErrorID |
|
- |
L_IE1P_Error |
|
|
|
|
|
Position |
|
- |
ARRAY [1..12] OF LREAL |
|
|
|
|
|
|
|
|
|
Inputs
|
Name Data type |
Information/possible settings |
|
|---|---|---|
|
AxesGroup AXES_GROUP_REF |
axes group reference |
|
|
ENABLE BOOL |
TRUE |
Read current position of the axes group continuously. |
|
CoordSystem |
Selection of the coordinate system to be used:
|
|
Outputs
|
Name Data type |
Value/meaning |
|
|---|---|---|
|
Valid BOOL |
TRUE |
Valid values are applied to the FB outputs. |
|
Busy BOOL |
TRUE |
Processing is running. |
|
Error BOOL |
TRUE |
An error has occurred. For details see ErrorID . |
|
ErrorID |
If Error = TRUE: Error number for the error that has occurred.
|
|
|
Position ARRAY [1..12] OF LREAL |
Current position of the axes group: |
|
Coordinate systems and transformations