MC_ReadAxisError

In addition to error messages of FBs, this FB serves to read error messages of the axis that are not assigned to special function blocks (e.g. device or communication errors).

 

 

 

MC_ReadAxisError

 

 

 

AXIS_REF

-

Axis

Valid

-

BOOL

BOOL

-

ENABLE

Busy

-

BOOL

Error

-

BOOL

ErrorID

-

L_IE1P_Error

AxisWarning

-

BOOL

AxisError

-

BOOL

AxisErrorID

-

L_IE1P_Error

InstanceName

-

STRING

TimeStamp

-

TIME

DriveWarning

-

BOOL

DriveError

-

BOOL

DriveErrorID

-

DWORD

STOActive

-

BOOL

VoltageEnabled

-

BOOL

MotorMagnetised

-

BOOL

QSPApplActive

-

BOOL

QSPDriveActive

-

BOOL

 

 

 

 

 

 

 

 

Inputs

Name

Data type

Information/possible settings

Axis

AXIS_REF

Transfer of the axis data structure

Motion axes (AXIS_REF)

ENABLE

BOOL

TRUE

Read actual error message of the axis continuously.

Outputs

Name

Data type

Value/meaning

Valid

BOOL

TRUE

Valid values are applied to the FB outputs.

Busy

BOOL

TRUE

Processing is running.

Error

BOOL

TRUE

An error has occurred.

For details see ErrorID .

ErrorID

L_IE1P_Error

If Error = TRUE: Error number for the error that has occurred.

AxisWarning

BOOL

TRUE

An error has occurred in the axis data or a connected function block that does not lead to a change to the " ErrorStop " axis state.

For details see AxisErrorID .

AxisError

BOOL

TRUE

An error has occurred in the axis data or a connected function block that leads to a change to the " ErrorStop " axis state.

For details see AxisErrorID .

AxisErrorID

L_IE1P_Error

If AxisError = TRUE: Error number for the error that has occurred.

If AxisWarning = TRUE: Error number for the warning that has occurred.

Error number for the error that has occurred

InstanceName

STRING

Instance name of the error origin

TimeStamp

TIME

Time of occurrence of the active error

DriveWarning

BOOL

TRUE

There is a warning in the inverter.

DriveError

BOOL

TRUE

There is an error in the inverter.

For details see DriveErrorID .

DriveErrorID

DWORD

If DriveError = TRUE: Error number for the error that has occurred