MC_Reset

This FB serves to reset an error message currently available in the axis (if the reason for the error is removed). If no more errors are pending, the axis changes from the " ErrorStop " axis state to the " Standstill " or " Disabled " axis state.

 

 

 

MC_Reset

 

 

 

AXIS_REF

-

Axis

Done

-

BOOL

BOOL

-

Execute

Busy

-

BOOL

Error

-

BOOL

ErrorID

-

L_IE1P_Error

 

 

 

 

 

 

 

 

Inputs

Name

Data type

Information/possible settings

Axis

AXIS_REF

Transfer of the axis data structure

Motion axes (AXIS_REF)

Execute

BOOL

TRUE

Reset (acknowledge) error message.

Outputs

Name

Data type

Value/meaning

Done

BOOL

TRUE

Axis is in the " Standstill " or " Disabled " axis state.

Busy

BOOL

TRUE

Processing is running.

Error

BOOL

TRUE

An error has occurred. For details see ErrorID .

ErrorID

L_IE1P_Error

If Error = TRUE: Error number for the error that has occurred.