MC_CamIn
This FB serves to execute a provided cam.
- For clutching to the master axis, the slave axis carries out a compensating movement.
- Various modes are available for the clutch-in process.
- For master and slave axis, an extension/compression and offset can be activated.
- Only the slave axis is moved with this FB, not the master axis.
|
|
|
|
MC_CamIn |
|
|
|
|
|---|---|---|---|---|---|---|---|
|
AXIS_REF |
- |
|
Master |
InSync |
|
- |
BOOL |
|
AXIS_REF |
- |
|
Slave |
Busy |
|
- |
BOOL |
|
BOOL |
- |
|
Execute |
Active |
|
- |
BOOL |
|
BOOL |
- |
|
ContinuousUpdate |
CommandAborted |
|
- |
BOOL |
|
BOOL |
- |
|
DirectChange |
Error |
|
- |
BOOL |
|
LREAL |
- |
|
MasterOffset |
ErrorID |
|
- |
L_IE1P_Error |
|
LREAL |
- |
|
SlaveOffset |
EndOfProfile |
|
- |
BOOL |
|
LREAL |
- |
|
MasterScaling |
|
|
|
|
|
LREAL |
- |
|
SlaveScaling |
|
|
|
|
|
LREAL |
- |
|
MasterStartDistance |
|
|
|
|
|
LREAL |
- |
|
MasterSyncPosition |
|
|
|
|
|
LREAL |
- |
|
ClutchTime |
|
|
|
|
|
LREAL |
- |
|
VelocityDiff |
|
|
|
|
|
LREAL |
- |
|
Acceleration |
|
|
|
|
|
LREAL |
- |
|
Decelerartion |
|
|
|
|
|
LREAL |
- |
|
Jerk |
|
|
|
|
|
MC_START_MODE |
- |
|
StartMode |
|
|
|
|
|
L_MC2P_
|
- |
|
ScalingOffsetMode |
|
|
|
|
|
MC_SOURCE |
- |
|
MasterValueSource |
|
|
|
|
|
BOOL |
- |
|
Periodic |
|
|
|
|
|
BOOL |
- |
|
MasterAbsolute |
|
|
|
|
|
BOOL |
- |
|
SlaveAbsolute |
|
|
|
|
|
MC_CAM_REF |
- |
|
CamTable |
|
|
|
|
|
MC_BUFFER_MODE |
- |
|
BufferMode |
|
|
|
|
|
|
|
|
|
|
|
|
|
Inputs
|
Name Data type |
Information/possible settings |
|
|---|---|---|
|
master |
Transfer of the axis data structure of the master axis |
|
|
Slave |
Transfer of the axis data structure of the slave axis |
|
|
Execute BOOL |
FALSE ä TRUE |
Clutch in slave axis and execute cam.
|
|
ContinuousUpdate BOOL |
Continuous acceptance of the parameters |
|
|
FALSE |
The pending parameters are accepted with a rising edge at Execute . |
|
|
TRUE |
The pending parameters are accepted continuously, i.e. during the execution the parameters may change. |
|
|
DirectChange BOOL |
TRUE |
An immediate cam replacement is permitted. |
|
MasterOffset LREAL |
Offset in [unit] for shifting the master position
|
|
|
SlaveOffset LREAL |
Offset in [unit] for shifting the slave position
|
|
|
MasterScaling LREAL |
Factor for rescaling the master axis
Note: The factor must not become negative! |
|
|
SlaveScaling LREAL |
Factor for rescaling the slave axis
Note: The factor must not become negative! |
|
|
MasterStartDistance LREAL |
Distance via which the clutch-in process is executed. |
|
|
MasterSyncPosition LREAL |
Position of the master axis where the clutch-in process ends. |
|
|
ClutchTime LREAL |
Time period for smooth clutching-in via time clutch |
|
|
VelocityDiff LREAL |
Maximum velocity difference in [unit/s] Max. velocity of the compensating movement, i.e. only specify if START_MODE.mcLimited applies. |
|
|
Acceleration LREAL |
Maximum acceleration in [unit/s 2 ] Max. acceleration of the compensating movement, i.e. only specify if START_MODE.mcLimited applies. |
|
|
Deceleration LREAL |
Maximum deceleration in [unit/s 2 ] Max. deceleration of the compensating movement, i.e. only specify if START_MODE.mcLimited applies. |
|
|
Jerk LREAL |
Maximum jerk in [unit/s 3 ] Max. jerk of the compensating movement, i.e. only specify if START_MODE.mcLimited applies. |
|
|
StartMode |
Type of clutch-in:
|
|
|
ScalingOffsetMode |
Scaling and offset mode:
|
|
|
MasterValueSource |
Source of relevant data for the master axis:
|
|
|
Periodic BOOL |
Selection is periodic/not periodic |
|
|
FALSE |
Curve is not periodic |
|
|
TRUE |
Curve is periodic (default if input is not connected) |
|
|
MasterAbsolute BOOL |
Selection is absolute/relative for master |
|
|
FALSE |
Master is relative |
|
|
TRUE |
Master is absolute (default if input is not connected) |
|
|
SlaveAbsolute BOOL |
Selection is absolute/relative for slave |
|
|
FALSE |
Slave is relative |
|
|
TRUE |
Slave ist absolute (default if input is not connected) |
|
|
CamTable MC_CAM_REF |
Transfer of the generated cam data |
|
|
BufferMode |
Mode for processing successive motion commands Note: Only the mcBuffered and mcAborting buffer modes are supported. |
|
Outputs
|
Name Data type |
Value/meaning |
|
|---|---|---|
|
InSync BOOL |
TRUE |
Slave and master axis are synchronised, the work curve is executed. |
|
Busy BOOL |
TRUE |
Processing is running. |
|
Active BOOL |
TRUE |
The command of the FB is currently executed.
|
|
CommandAborted BOOL |
TRUE |
The command was aborted by another FB.
|
|
Error BOOL |
TRUE |
An error has occurred. For details see ErrorID .
|
|
ErrorID |
If Error = TRUE: Error number for the error that has occurred.
|
|
|
EndOfProfile BOOL |
FALSE ä TRUE |
Cyclic end of the cam profile reached. The TRUE state is only set for one cycle (pulsed signal). |
Motion axes (AXIS_REF)