MC_PhasingRelative
This FB serves to set a virtual relative offset between the applied master axis and the applied slave axis. The special feature here is that the offset only exists virtually and this FB does not cause any motion control.
- From the view of the slave axis, the virtual offset is located on the master axis without the master axis noting it.
- As soon as an FB for multi-axes movements ( MC_CamIn , MC_GearInPos , ...) is called with the same master slave configuration, the virtual offset is considered automatically.
- An offset set via MC_PhasingRelative can be deleted by means of the L_MC2P_ResetPhasing function block without having any impact on the movement of the axis which has been uncoupled in the meantime again.
|
|
|
|
MC_PhasingRelative |
|
|
|
|
|---|---|---|---|---|---|---|---|
|
AXIS_REF |
- |
|
master |
Done |
|
- |
BOOL |
|
AXIS_REF |
- |
|
Slave |
Busy |
|
- |
BOOL |
|
BOOL |
- |
|
Execute |
Active |
|
- |
BOOL |
|
LREAL |
- |
|
PhaseShift |
CommandAborted |
|
- |
BOOL |
|
LREAL |
- |
|
Velocity |
Error |
|
- |
BOOL |
|
LREAL |
- |
|
Acceleration |
ErrorID |
|
- |
L_IE1P_Error |
|
LREAL |
- |
|
Deceleration |
CoveredPhaseShift |
|
|
LREAL |
|
LREAL |
- |
|
Jerk |
|
|
|
|
|
MC_BUFFER_MODE |
- |
|
BufferMode |
|
|
|
|
|
|
|
|
|
|
|
|
|
L_MC2P_ResetPhasing