Menu ribbon

The ribbon groups the functions of the IDE into menus and groups.

The ribbon is located at the top of the development environment.

Ribbon with the active start menu

The ribbon provides the following menus:

File

The file menu provides functions for creating, managing, editing or importing projects.

Start

The menu provides editing functions such as copying and pasting as well as the toolbox with control elements and functions.

View

You can use the menu functions to display closed windows such as the project explorer or the document organisation again.

Project

The project menu provides functions for creating projects, editing them in external tools and transferring them to the target system.

Tools

The tools menu provides settings for the build configuration and access to the Options dialogue.

Help

The help menu provides »EASY UI Designer«help and information on the installed »EASY UI Designer« version.

Context menu of the ribbon and the quick access toolbar

A context menu with the following functions is available for each function in the ribbon and in the quick access toolbar:

After restarting the development environment, these changes are lost.