EASY UI Designer

The »EASY UI Designer« is a Lenze software tool for creating web-based machine visualisations in combination with the Fast UI Runtime on the c520, c550 and c430 controllers.

It requires no programming knowledge in web development, as it is configured with ready-made templates and controls.

The »EASY UI Designer« is based on the "VisiWin 7" tool from INOSOFT GmbH(www.inosoft.com) and has been extended by Lenze with its own components and templates.

Project configurator

When you start »EASY UI Designer«, the project configurator is displayed.

Quick start

Practical instructions to help you get started and familiarise yourself with the most important functions of »EASY UI Designer«.

Project management

From the initial creation of the project on the development computer to commissioning on the runtime system, there are various project-related tasks in which you are supported by the »EASY UI Designer« development environment and the supplied help tools.

System modules

Detailed description of the extensive visualisation-specific functions of »EASY UI Designer« such as variables, alarms, language switching, etc.

Design

The interface is developed using HTML and JavaScript technologies. It can therefore be displayed in any modern web browser on any end device.

Translation manager

The scope of delivery of »EASY UI Designer« includes auxiliary tools such as the translation manager.

Parameters of the system modules

Detailed descriptions of individual parameters, menu items and settings.

EASY UI Designer development environment

Get to know the user interface of the "EASY UI Designer" development environment in detail.

Parameter reference of the system modules

Detailed description of all system module parameters.