System modules
The following system modules are available:
Defines the connection information of the application. Defines which devices are addressed and which data is exchanged and how.
Defines the function of individual process variables with regard to alarm functionality. Defines how the individual alarms are displayed and how they are processed by the system and user.
Determines which process variables are recorded and displayed in X/t or XY graphs.
Affects all displayed texts within the application. The multilingual configuration of the texts used allows the language to be switched at runtime without additional effort.
Defines user groups and rights and sets permissions for individual functions.