Authorisation level

In level-oriented user administration, the authorisation level is used to determine which authorisation level users in this user group have. Control elements can be assigned an authorisation level via the Authorisation property. If the value of this property is less than or equal to the authorisation level of the user currently logged in, the control element is enabled for input.

Level-oriented user management is based on the following principle: an employee hierarchy can be created using the authorisation level and the AuthorisationRight property. The higher the authorisation level of a user, the more approvals they can receive if the AuthorisationRight value of the input elements in the application is distributed accordingly.

Parameters for module: