Browser properties

Contains information that the browser needs to read variable information. The browser component defined via Browser has the option of saving its own configuration settings here. Both the format and the display via a dialogue are individual features of the browser component. A description can therefore be found in the corresponding documentation.

If the browser component stores its configuration values in this field, the corresponding configuration dialogue can be called up via the button.

Note: The standard OPC browser VisiWin7.Opc.Brw.dll stores the name of the OPC server used for browsing here, for example. This can therefore be a different OPC server than the one used for communication. A different OPC server can be selected via the button.

Parameters for module: