Max. count per file

Defines the maximum number of entries per file.

The value 0 means that the number of entries is irrelevant. This setting cannot be changed.

As soon as the specified number of entries is reached, a new archive file is created, even if the specifiedfile change event has not yet occurred. The value 0 means that the number of entries is irrelevant.

Example:

Parameters

Setting

Max. Number per file

1000

File change event

Time period, 1 day

On 6 March at 14:00, the 1000th entry is written to the existing archive file. According to the setting for the file change event, a new file should not be created until 7 March at 00:00. However, a new file is created after the 1000th entry.

Parameters for module: