Variable for transmission trigger
Defines a variable whose value change to 1 triggers the sending of values from a recipe file directly to the variable server. The recipe buffer is not affected by this function. After sending, the value of the variable is automatically reset to 0. The variable can have either a Boolean or an integer data type. The bit serving as the trigger is then selected by specifying the bit number in the variable selection dialogue.
The name of the file to be loaded is expected in a process variable, which must be specified in the file name variable parameter.
Parameters for
- Recipes module:
- Recipe class