File name variable

Also: Variable for file name

Determines which variable of data type VT_BSTR contains the recipe file name. The recipe is saved/loaded under this name. This parameter has a different function depending on the object:

Recipe class

The content of the variable for file name ( Automation tab of the property pages) is only used if the trigger functions are triggered via the variables for loading, sending and saving the recipe definition. When using an IRecipeClass object, the file name variable has no function.

Sub-recipe element

The data of a sub-recipe can either be saved as a separate file or in the parent recipe. If the Save sub-recipe class values here parameter is activated, the File name variable parameter has no meaning.

Parameters for

Recipes module:
RecipeclassSubrecipeelement

See also