Variable for memory trigger

Defines a variable whose value change to 1 triggers the saving of values from the recipe server to the recipe file. After saving, the value of the variable is automatically reset to 0. The variable can have either a Boolean or an integer data type. The bit serving as the trigger is then selected by specifying the bit number in the variable selection dialogue.

The name of the file to be saved is expected in a process variable, which must be specified in the file name variable parameter.

Parameters for

Recipes module:
Recipe class

See also