Sub-recipe element

In a recipe class, recipe elements are used to define which data belongs to this recipe.

A sub-recipe element refers to another recipe class that is integrated into this recipe. The type of integration is defined by the parameter Save sub-recipe class values in this recipe class in this recipe definition. This makes it possible to nest several recipe definitions. The special features are described in more detail in the chapter .

Parameters

Name Description of the
File name variable Determines the variable that contains the recipe file name.
Definition active Determines whether the object definition is valid. (only Cross-Platform Server)
Comment Optional commentary on the object.
Sort index Defines the order of the recipe elements.
Sub-recipe class Inserts a recipe class as a recipe element.

See also