Time until automatic logout

Determines the time after which a user is automatically logged off if the HMI is not operated.

Specifies the period (in minutes) after which a user is automatically logged off if the HMI is not operated. If a user forgets to log off after using the HMI, this occurs automatically after the period specified in the parameter Time until automatic logoff. This prevents operation from accidentally remaining enabled after a user has already left the workstation.

If the parameter is set to 0, there is no automatic logout.

Parameters for module: