Replace {language} placeholder
Defines which identifier of the target language is formatted into the file name.
When selecting the file name for the export, the placeholder "{language}" was added to the file name. This is replaced by the following setting when exporting in order to generate a unique file name for each target language.
-
This setting is only available if Create a file for each target language is selected.
|
Setting |
Description of the |
|---|---|
|
Voice recognition Command line: "Lcid" |
The language identifier, also known as the "LCID" (locale identifier), is a unique number and is defined by the Windows operating system.
|
|
Language abbreviation Command line: "Name" |
The language abbreviation consists of an abbreviation for the language and possibly an abbreviation for the country.
|
|
Windows language abbreviations Command line: "ThreeLetterWindowsLanguageName" |
The Windows language abbreviation "ThreeLetterWindowsLanguageName" consists of 3 letters for a language and is defined by the Windows operating system.
|