On the property pages, you can display and change the parameters of the definition of a VisiWin system module selected in the table editor or in the project explorer.
In the Property pages window, you can configurethe projectand set parameters for definitions of the VisiWin system modules. In the standard window layout, the Property pages window is located at the bottom of the user interface.
If the window is too small to display all tabs, buttons are displayed at the bottom left of the window instead, which are used to scroll between the tabs.