Configure project

EASY UI Designer projects contain settings that affect the runtime behaviour of the project. Some of these settings are already offered when a project is created, e.g. programming language or project type. Other settings can be edited after the project has been created.

To edit the project configuration settings:

  1. In the project explorer, select the Project configuration node of the project that you want to configure.
    The project explorer organises the available configuration parameters into different areas, which are displayed as sub-nodes, e.g. target device, global, application, etc.
    Note: The available configuration parameters depend on the project type.
  2. Click on an area that you want to configure.
    The corresponding parameters are displayed in the Property pages window. The parameters are categorised again here and offered for editing on various tabs, e.g. Advanced, Language etc.
    Note: Some configuration parameters such as project type or designer (programming language) cannot be edited as they were already defined when the project was created.
  3. Setthe configuration parameters as required.