Call up keyboard dialog

There are two different keyboards (alphanumeric/numeric) that can be connected to input elements such as the NumericVarIn and the TextVarIn if required. To do this, the dialogs "AlphabeticalKeyboardDialog.html" and "NumericKeyboardDialog.html" must be stored in the client folder under dialogsWkeyboards.

The call of the corresponding dialog is configured on the control element itself by linking the action "Lenze.Actions.ShowKeyboardDialogAction" to the ControlEventTrigger (see Show dialog). Depending on the element type, the alphanumeric or numeric keyboard is displayed at runtime by clicking on the input field.