Project templates

EASY UI Designer provides various templates that serve as the basis for new projects. Availability also depends on the installation, any available additional installation and the development licence.

In the development environment, the available templates are listed on the File > New project page. The possible templates are filtered there by selecting the VisiWin version, UI technology and programming language.

Template Version UI Programming language Notes
Client
  • from 7.0
  • from 7.2
  • as of 7.2 SP7
  • Modern UI
  • Classic UI
  • Web UI
  • C#, VB.NET
  • C#, VB.NET
  • JavaScript
Group from 7.0 An empty project group into which further projects must be loaded.

This template is independent of the UI technology and the programming language, as it does not contain a graphical user interface.

Server from 7.0 This template is independent of the UI technology and the programming language, as it does not contain a graphical user interface.
Server/client
  • from 7.0
  • from 7.2
  • as of 7.2 SP7
  • Modern UI
  • Classic UI
  • Web UI
  • C#, VB.NET
  • C#, VB.NET
  • JavaScript
A project group that contains a server project and a client project. The client project is already configured to access the server project. Additional projects can be added to this project group at any time.
Single
  • from 7.0
  • from 7.2
  • Modern UI
  • Classic UI
  • C#, VB.NET
  • C#, VB.NET
Plugin Configuration from 7.2 Modern UI C#
Plugin from 7.2 Modern UI C# You can only select this template when you add a new project to an existing plugin configuration.
Shell from 7.2 Modern UI C# You can only select this template when you add a new project to an existing plugin configuration.
SystemPlugin from 7.2 Modern UI C# You can only select this template when you add a new project to an existing plugin configuration.

See also