Max. file count
Specifies the maximum number of archive files that can be created on the hard drive by the archive definition. If the number specified here is exceeded, the oldest archive files are deleted. This serves to protect the hard drive from overflowing.
The maximum number of files is limited to 28 and cannot be changed.
An additional method for limiting the archive data on the hard drive is made possible via the Max. Total file size parameter.
Parameters for module: