Max. files size

Specifies the maximum storage space that the archive files of the archive definition may occupy. If the size specified here (in kilobytes) is exceeded, the oldest archive files are deleted. This serves to protect the hard drive from overflowing.

The maximum total file size is limited to 40,000 kB and cannot be changed.

An additional method for limiting the archive data on the hard drive is made possible via the Max. Number of files parameter.

Parameters for module: