Concepts and basics (system module recipes)
- Recipe definition
- A recipe definition, also known asa recipe class, specifies all the parameters that need to be set for the manufacture of a product.
- Recipe data
- The data of an individual recipe consists of variables, information blocks, notes and a change history.
- Data storage
- The data of a recipe is processed and stored at various locations.
- Data transmission
- The transfer of recipe data between the different storage locations can be controlled individually.
- Data display and input
- Using a switch, a control element in the client can either access the original value from the variable server or the value in the recipe buffer.
- Recipe class object
- The recipe class object in the VisiWin API provides programmatic access to a recipe class.