Triggers and actions

Learn more about triggers and actions, what they are used for and which triggers and actions are available.

A control can execute additional functions (actions) after an event, e.g. show a dialog if the user clicks on the control. To do that, a control needs a trigger such as a click event.

Trigger

A trigger triggers an action in a control.

The following triggers are available:

Actions

An action is a function that is executed upon an event defined by the trigger, e.g. a user input or a variable value change.

The Add Action dialog shows all available actions. All actions have a tool tip describing the selected action. To show the tool tip in the dialog, hold your mouse above the name of the action you want to know more about. The tool tip appears shortly after.