Page

A page is a page that shows the actual content of the visualisation. An example is a diagnostics page for the machine (DiagnosticsPage.html).

Pages are loaded into the "AppPageNavigator" (container into which any page can be loaded), which may only exist once in an app. The "AppPageNavigator" contains the main navigation.

A new project already contains the following pages:

CurrentAlarmsPage.html

Overview of current alarms. It contains an alarm list that is filled with the current alarms at runtime.

DiagnosticsPage.html

Template for diagnostic information. Provide users with information on diagnosing errors here.

HistoricalAlarmsPage.html

Overview of historical alarms. It contains the list of historical alarms.

LoadingPage.html

Includes the LoadingSpinner control to indicate that a page is still loading. The LoadingPage is displayed at runtime instead of the actual page until that page is loaded. To enable the display of the LoadingPage, the ShowLoadingSymbol property of the control navigating to the actual page must be enabled.

MachinePage.html

Template for the machine overview. You can design the start page of your machine here.

RecipesPage.html

Template for recipe management. It contains the recipe management template if the recipe function has been activated in the project configurator.

SettingsPage.html

Template for settings. You can add generic settings here.

StatisticsPage.html

Template for statistics. This page can be filled with statistics or performance indicators for your machine.

Related topics: