LoadingSpinner

Animated element to indicate a loading process.

The LoadingSpinner is used to make apparent to the user that the desired contents are loading.

The LoadingSpinner is already included in the LoadingPage.html and the LoadingView.html. A loading spinner can also be configured for the TrendChart control.

The LoadingPage with a LoadingSpinner (two arches rotating around a center point) is displayed while the actual page is loading.

Functionalities

The control supports the following functionality:

To configure the following functionalities, select the control in the designer or in the Document Outline and set the properties in the Properties window. The IDE shows a tool tip for each property describing the selected property. To show the tool tip, hold your mouse above the name of the property you want to know more about in the Properties window. The tool tip appears shortly after.

Anatomy

The control contains a number of child elements. Both the control itself and its child elements can be configured using the properties of the control. The properties of a child element are usually found in the category named after this child element.

The properties configuring the Spinner element are found in the Spinner category in the Properties window if you select the control in the designer or in the Document Outline.

The LoadingSpinner and its elements

Animation (Spinner)

To configure the animation, use the properties found in the Spinner category. The SpinnerType property allows to select the type of animation you want to use. The SpinnerWidth and SpinnerHeight properties set the width and height of the element. To play the animation, use the PlayAnimation property.