View
A view is a specific view that can be used multiple times in the visualisation.
A view is placed in a region that can exchange views at runtime. One example is a view with navigation buttons (ButtonView.html). Encapsulation in a view enables flexible replacement of the navigation buttons during operation.
A new project already contains the following views:
The AppShell.html file defines the main view of the visualisation. It contains the basic layout of the visualisation, which consists of at least one menu and the AppPageNavigator.
ButtonView.html, HeaderView.html
Menu views. Depending on the project layout, parts of the menu are shown in these views.
ErrorView.html
Error view. View for displaying errors during runtime. This page should not be manipulated.
Includes the LoadingSpinner control to indicate that a view is still loading. The LoadingView is displayed at runtime instead of the actual view until that view is loaded. To enable the display of the LoadingView, the ShowLoadingSymbol property of the control navigating to the actual view must be enabled.
LoginView.html
Login view. It contains the login window for visualisation.
Related topics: