Group

Monitoring groups are displayed in the project explorer under the main access node. Monitoring groups can be nested hierarchically. The maximum nesting depth is eight.

Monitoring groups include the following functionality:

  • You define the monitoring type of the monitoring configured directly under the group.
  • They enable the hierarchical structuring of information.
  • They enable the hierarchical deactivation of all subordinate monitoring definitions at runtime.

Parameters

Name Description of the
Bit number Defines the bit within the variable that triggers the function.
Deactivation variable Variable for switching on/off all monitoring contained in the group (at runtime)
Definition active Determines whether the object definition is valid.
Comment Optional commentary on the object.
Name Name of the object.
Type Defines the monitoring type.

See also