Import texts

The import is used to transfer the texts returned by the translator from the returned file (import file) into the project file.

Once all the data has been entered on the File, Languages and Options tabs, the function is triggered with the Import button. A message then displays the success or the errors are listed in detail (see Error display).

Results for the set data are displayed on the Statistics tab.

The import is only limited to the existing texts in the project file. If new texts are added to the import file, these are not inserted into the project file!

The translation manager is not an alternative to the language switch editor. If you want to exchange or add texts between several projects or between a project and an external file, use the "Copy" and "Paste" functions via the Windows clipboard in the development system instead.

File

Setting

Description of the

File with languages to be imported

Complete file name of the import file.

Click on or double-click on the text box to open a file selection dialogue.

From clipboard

Instead of a file, text from the clipboard can also be used for the import. This button is used to import it and display it in the text box. Any previously selected file name is deleted. The text box can be deleted again using the Loeschen.Protection button.

Languages

Setting

Description of the

Source language

Specification of the source/outgoing language.

  • The language is automatically recognised from the file to be imported.

Target languages to be imported

Specification of the target languages that have been translated and are now to be imported into the project.

  • The languages are automatically recognised from the file to be imported.

Import source language

Also imports the source language into the project.

Options

Setting

Description of the

Import all texts

Only import texts that are empty in the project

Defines which texts are to be imported.

Only import texts that are identical in the source language in the project and in the import file

Texts are only imported if the source language texts match.

Only import texts with correct text parameters

Texts are only imported if the number, numbering and type of the text parameters are correct.

Statistics

The table shows how many text groups and texts were found in the import file(s) for which languages.

Language selection dialogue

To import texts, the files containing the texts to be imported must be specified. It can happen that the target language is no longer saved in the import file. This sometimes happens with Xliff files that are written by external translation tools. The translation manager then tries to determine the target language based on the file name. If this is also not possible, the user is asked which language the import file contains.

Setting

Description of the

OK

The target language must first be selected from the list.

Cancel

The target language cannot be recognised. The file is then ignored for the import.