Import source language
Also imports the source language into the project.
Normally, only target languages are imported into a project. The source language may be used as a reference. However, if the source language has also been changed in the import file, e.g. by editing, the source language can be imported back into the developer language using this option.
-
This option is only visible if the option Treat source language as target language has been activated in the programme settings.
-
If this option is used, the option Only import texts that are identical for the source language in the project and in the import file is automatically deactivated on the Languages tab.