FixClassical

The FixClassical layout has a header and a series of navigation buttons at the bottom of the screen that can be used to call up the various pages of the machine visualisation. Elements can only be positioned absolutely, so this layout is only suitable for display sizes with a similar resolution.

The buttons (user) and (settings) in the header refer to the server-side user management and language switching functions.

Document outline

The associated main view "AppShell.html" contains the following elements in the document structure.

HeaderRegion

The HeaderRegion contains the header. By default, the "HeaderView.html" view is displayed in this region.

AppPageNavigator

The AppPageNavigator displays the various pages with the actual content at runtime. Therefore, do not insert any elements in this area, but create the visualisation on the respective page, for example "MachinePage.html".

ButtonRegion

The ButtonRegion contains the buttons for navigation. By default, the "ButtonView.html" view is displayed in this region.

All user interfaces of the project are contained in the client folder under "Design". Double-click on an entry to open the corresponding file in the Designer workspace.

Header

The "HeaderView.html" view defines the header of the application.

Navigation buttons

The ButtonView.html view defines the buttons for navigation.

Related topics: