Value label

Display of the variable value and the unit in the control element.

The display of a variable value as text or number is a main functionality of the input and output control elements. A "Display for value and unit" (ValueLabel) can be configured for graphical input and output controls(Bar, DonutGauge and Slider), which acts as a container for the value and unit.

The "ValueLabel" element is contained in the "Bar" control element, for example.

The following properties are available in the "ValueLabel" category to configure this display:

ShowValueLabel

Determines whether the display for value and unit is shown.

ValueLabelBorderRadius

Defines the thickness of the rounding of the corners for the frame of the display for value and unit.

ValueLabelBorderStyle

Defines the type of display frame for the value and unit.

ValueLabelBorderWidth

Defines the thickness of the frame line of the display for value and unit.

ValueLabelHeight

Defines the height of the display for value and unit.

ValueLabelMargin

Defines the outer distancesof the display for value and unit, i.e. between the edge of the display and its parent element and its neighbouring elements.

ValueLabelPadding

Defines the inner distancesbetween the display for value and unit and its content (value and unit).

ValueLabelPosition

Defines the position of the display for value and unit within the control element.

ValueLabelWidth

Defines the width of the display for value and unit.

Affects these controls:

Bar, DonutGauge, Slider