Export texts
The export creates one or more files in a standard format that contain the localised texts to be translated from the project. These files are passed on to the translator(s).
Once all the data has been entered on the File, Languages and Options tabs, the function is triggered with the Export button. A message then displays the success or the errors are listed in detail (see Error display).
Results for the set data are displayed on the Statistics tab.
|
Setting |
Description of the |
|---|---|
|
Defines the file type for the texts to be exported. |
|
|
Specifies whether a file with all target languages or a file for each target language should be created. |
|
|
Complete file name for the export file. Click on |
|
|
Defines which identifier of the target language is formatted into the file name. |
|
|
Defines the type of column headings for the languages. |
|
|
The nesting of the text groups is resolved into a flat list. |
Supported combinations:
|
File type |
One file per target language |
{language} placeholder |
Column naming |
Store hierarchy flat |
Number of languages |
|---|---|---|---|---|---|
|
ExcelX |
x |
x |
x |
2 |
/ |
|
Excel |
x |
x |
x |
2 |
max. 3 |
|
Text |
x |
x |
x |
2 |
/ |
|
XLIFF |
x 1 |
x |
- |
x |
/ |
|
Clipboard |
- |
- |
x |
2 |
/ |
|
x |
Is supported |
|
- |
Not supported |
|
/ |
No restriction |
|
1 |
Only this format |
|
2 |
Always this attitude |
|
Setting |
Description of the |
|---|---|
|
Specification of the source/outgoing language. |
|
|
Specify the target languages for which a translation is to be made. |
|
|
Languages that can be exported to the files in addition to the target languages. |
|
|
|
Moves the selected language to the top. When exporting to a column-based file (Excel/text), the different languages are saved next to each other. The order is: source language, target languages, additional languages. |
|
|
Moves the selected language down. |
|
|
Selects all languages. |
|
|
Deselects all languages. |
The four buttons affect the previously clicked list of languages.
|
Setting |
Description of the |
|---|---|
|
Opens a dialogue in which the text groups to be exported can be selected. |
|
|
Displays the selected text groups. The number of groups including subgroups and the number of texts is displayed in brackets. |
|
|
If the text in the developer language is empty, the text definition is ignored when exporting. |
|
|
Defines which texts are to be exported. |
|
Setting |
Description of the |
|---|---|
|
Number of text groups |
Displays the total number and the number of selected text groups. |
|
Number of texts |
Displays the total number and the number of texts to be exported for each target language. |
or double-click on the text box to open a file selection dialogue.