The controls for Web UI are provided in the EASY UI Designer toolbox and are divided into different categories.
| Category | Symbol and name | Description of the |
|---|---|---|
| Buttons | Contains control elements that trigger a function or change a process variable when operated. | |
Button |
Button for calling up a function. | |
ToggleButton |
Switch for switching an option on or off . | |
Key |
Push-button with variable connection. | |
Switch |
Switch for switching an option on or off . | |
CheckBox |
Checkbox for activating or deactivating an option. | |
RadioButton |
Element for activating or deactivating an individual option from a group of options. | |
RadioButtonGroup |
Control element for grouping options, only one of which can be activated at a time. | |
| Input/output | Contains control elements for the input and output of process values. | |
DropDownBox |
Expandable list of options from which only one can be selected. | |
SelectBox |
Control element with drop-down menu for selecting an element. | |
ListBox |
Control element for displaying a static or runtime-generated list. | |
NumericVarOut |
Output field for a numerical process variable . | |
TextVarOut |
Output field for an alphanumeric process variable . | |
Bar |
Bar chart for displaying a process variable value . | |
RadialInstrument |
Tachometer-like display of a process variable value . | |
DonutGauge |
Ring diagram for displaying a process variable value . | |
PieChart |
Pie chart for displaying multiple values . | |
StackedDonutGauge |
Ring diagram for displaying multiple variable values . | |
NumericVarIn |
Input/output field for a numerical process variable value . | |
TextVarIn |
Input/output field for an alphanumeric process variable value. | |
DateTimeVarIn |
Input/output for a date and/or a time . | |
Slider |
Slider for the input and output of a variable value . | |
Label |
Display of a text and a symbol for labelling other elements. | |
TextBlock |
Display of a text. | |
Clock |
Clock, displays the system time. | |
Image |
Display of a graphic. | |
ColorIndicator |
Control element that changes colour when the value of the linked variable changes. | |
StateIndicator |
Control element that changes its colour, text and icon depending on the value of the linked variable. | |
VideoPlayer |
Control element for playing a video. | |
PDFViewer |
Control element for displaying a PDF document . | |
EmbeddedWebsite |
Control element for integrating an external resource into the application. | |
| System | Contains control elements for displaying data from the VisiWin 7 system modules. | |
AlarmList |
Display of alarms in the form of a table or list . | |
HistoricalAlarmList |
Display of historical alarms in tabular form. | |
AlarmIndicator |
Indicates the presence of alarms. | |
| Container | Contains controls that can accommodate other controls. | |
TabBar |
Bar with buttons for navigation. | |
AbsoluteLayout |
Container for manual positioning of control elements. | |
FlexLayout |
Container for automatic positioning of control elements . | |
CardLayout |
Container for automatic positioning of cards. | |
Card |
Control element that is displayed on a CardLayout, with a heading and content. | |
CardHeader |
Container for the heading of a card. | |
CardContent |
Container for the contents of a card. | |
Group |
Container for control elements with frame and labelling . | |
ViewBox |
Container for scaling the content. | |