Overview of the controls
The controls are provided in the toolbox of »EASY UI Designer«and are divided into different categories. You can find an overview here.
Buttons
Contains control elements that trigger a function or change a process variable when operated.
|
Symbol and name |
Description of the |
|---|---|
|
Button for calling up a function. |
|
|
Switch for switching an option on or off. |
|
|
Push-button with variable connection. |
|
|
Switch for switching an option on or off. |
|
|
Checkbox for activating or deactivating an option. |
|
|
Element for activating or deactivating an individual option from a group of options. |
|
|
Control element for grouping options, only one of which can be activated at a time. |
Input/output
Contains control elements for the input and output of process values.
|
Symbol and name |
Description of the |
|---|---|
|
Expandable list of options from which only one can be selected. |
|
|
Output field for a numerical process variable. |
|
|
Output field for an alphanumeric process variable. |
|
|
Output for a date and/or a time. |
|
|
Clock, displays the system time. |
|
|
Bar chart for displaying a process variable value. |
|
|
Bar chart consisting of segments for displaying a process variable value. |
|
|
Tachometer-like display of a process variable value. |
|
|
Pie chart for displaying multiple values. |
|
|
Diagram for displaying XY coordinates. |
|
|
Ring diagram for displaying a process variable value. |
|
|
Input/output for a date and/or a time. |
|
|
Input/output field for a numerical process variable value. |
|
|
Input/output field for an alphanumeric process variable value. |
|
|
Slider for the input and output of a variable value. |
|
|
Display of a text and a symbol for labelling other elements. |
|
|
Display of a graphic. |
|
|
Control element that changes colour when the value of the linked variable changes. |
|
|
Control element that changes its colour, text and symbol depending on the value of the linked variable. |
System
Contains control elements for displaying data from the system modules.
|
Symbol and name |
Description of the |
|---|---|
|
Alarm line that displays several alarm categories and can be expanded. |
|
|
Display of alarms in the form of a table or list. |
|
|
Display of historical alarms in tabular form. |
|
|
Indicates the presence of alarms. |
|
|
Control that displays trend data over time in a curve chart. |
|
|
Control that allows to interact with the to which it is connected TrendChart. |
|
|
Table containing information on curves of a TrendChart control. |
Layout
|
Symbol and name |
Description of the |
|---|---|
|
Container for manual positioning of control elements. |
|
|
Container for automatic positioning of control elements. |
|
|
Container for control elements with frame and labelling. |
|
|
Container for automatic positioning of cards. |
|
|
Control element that is displayed on a CardLayout, with a heading and content. |
|
|
Container for scaling the content. |
Navigation
|
Symbol and name |
Description of the |
|---|---|
|
Bar with buttons for navigation. |
|
|
A placeholder control that enables navigation through multiple views. |
Media
|
Symbol and name |
Description of the |
|---|---|
|
Control element for playing a video. |
|
|
Control element for displaying a PDF document. |
|
|
Control element for integrating an external resource into the application. |
Other controls
Some controls are not included in the ribbon but used in templates that are already included in each new project or can be added to the project if needed.
|
Name |
Beschreibung |
Vorlagen |
|---|---|---|
|
Animated element to indicate a loading process. |